Hi
I am working with MPC5748g LCEVB. I want to receive some data from a system via Ethernet. To send data I need to set the IP address. I want to know whether the MPC5748G LCEVB support layer3 (Network layer).
regards
Rahul Ramakrishnan
Hello,
microcontroller supports layer 2 of OSI model by hardware. Upper layers must be implemented in software, for example using TCI/IP stack.
In S32 Design Studio, there is an example of lwIP stack, which you can use.
Please install S32 Design Studio and the newest update, and then create lwIP project from example.
https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=S32-DS-E2002-0
S32 Design Studio for Power Architecture 2017.R1 - Updates 5 and 6 available
Regards,
Martin