i.MX RT 1502 QSPIFLASH Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT 1502 QSPIFLASH Boot

1,675 Views
zhangfengxuan
Contributor I

The default PIN MUX :

GPIO-SD-B1-06 -----> L3  ------> FLEXSPI-QSPI-SS0
GPIO-SD-B1-07 -----> L4  ------> FLEXSPI-QSPI-CLK

GPIO-SD-B1-08 -----> P3  ------> FLEXSPI-QSPI-DATA0

GPIO-SD-B1-09 -----> N4  ------> FLEXSPI-QSPI-DATA1

GPIO-SD-B1-10 -----> P4  ------> FLEXSPI-QSPI-DATA2

GPIO-SD-B1-11 -----> P5  ------> FLEXSPI-QSPI-DATA3

When I design the board,I change the PIN MUX  :

GPIO-AD-B1-15 -----> J14  ------> FLEXSPI-QSPI-SS0
GPIO-AD-B1-14 -----> G12 ------> FLEXSPI-QSPI-CLK

GPIO-AD-B1-13 -----> H11  ------> FLEXSPI-QSPI-DATA0

GPIO-AD-B1-12 -----> H12  ------> FLEXSPI-QSPI-DATA1

GPIO-AD-B1-11 -----> J13   ------> FLEXSPI-QSPI-DATA2

GPIO-AD-B1-10 -----> L13  ------> FLEXSPI-QSPI-DATA3

Now,i can not boot from the new PIN MUX QSPIFLASH,even can not connect to the flash.

Does someone know that how can i download my hex to the flash now?

Thanks!

I change the BOOTCFG[2:0] from 000b to 111b,but it can not boot from the secondary pinmux.

pastedImage_195.png

pastedImage_196.png

It dosen't work。Is this a BUG ? if not ,how can i configure the boot_cfg?

Need help,Please.

Thanks.

Tags (2)
0 Kudos
Reply
2 Replies

1,100 Views
jay_heng
NXP Employee
NXP Employee

You can also try this tool, with this tool, You can flash bare image into various boot devices easily and don't need to care about headers (ivt, boot data...)

GitHub - JayHeng/nxp-sec-boot-ui: A one-stop GUI tool to work with NXP MCU (Kinetis, i.MXRT, LPC) RO... 

0 Kudos
Reply

1,100 Views
igorpadykov
NXP Employee
NXP Employee

Hi  fengxuan

one can start debugging with hardware side:

check voltages and clocks using Hardware Development Guide for the

MIMXRT1050 Processor
https://www.nxp.com/docs/en/user-guide/MIMXRT1050HDUG.pdf
Check if QSPIFLASH is able to write/read using MCUXpresso.

If flash is operational, one can try to write boot image to it, check signals

with oscilloscope, use

MIMXRT1050-EVK MfgTool and QSPI Flash 

AN12183 How to Enable Debugging for FLEXSPI NOR Flash

https://www.nxp.com/docs/en/nxp/application-notes/AN12183.pdf 

When boot fails, check if ROM jumped to serial downloader mode

(it should be visible by MFG TOOL).

Attach jtag, check if boot settings are correct reading SRC_SBMR1,2 registers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply