How could/would flash-resident bootloader, direct boot option, and application calls to run_bootloader() work?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How could/would flash-resident bootloader, direct boot option, and application calls to run_bootloader() work?

1,504 Views
donwilley
Contributor II

I want my flash resident boot loader to be in flash starting at 0x00000000 where it runs each time the system is restarted.  When there is an application at 0x00008000, I want that to be run directly using the direct boot option of the boot loader.  The boot loader reference describes this option, and when configured in the BCA, I pass through the boot loader's initialization code into my application.  Both images were loaded separately with a debugger into flash.

Now I want the application to call the flash-resident boot loader, and based on documentation in section 2.6, I expect a pointer to the boot loader API tree at 0x0000001C (a location in the boot loader vector table) that will tell me how to find runBootloader() and other goodies available from the boot loader.  I don't see the pointer at 0x0000001C when I browse memory (it is zero as expected from the source in my startup.S file).  Not a big deal, I can add it.

.section .isr_vector, "a"
.align 2
.globl __isr_vector
__isr_vector:
.long __StackTop /* Top of Stack */
.long Reset_Handler /* Reset Handler */
.long NMI_Handler /* NMI Handler*/
.long HardFault_Handler /* Hard Fault Handler*/
.long 0 /* Reserved*/
.long 0 /* Reserved*/
.long 0 /* Reserved*/
.long g_bootloaderTree /* Reserved ( for g_bootloaderTree, I hope. location = 0x0000001C )*/
.long 0 /* Reserved*/

When I browse memory with the debugger, I find it does point at 

//! @brief Static API tree.
const bootloader_tree_t g_bootloaderTree = {.runBootloader = bootloader_user_entry,
.version = {.name = kBootloader_Version_Name,
.major = kBootloader_Version_Major,
.minor = kBootloader_Version_Minor,
.bugfix = kBootloader_Version_Bugfix },
.copyright = bootloaderCopyright,
.runtimeContext = &g_bootloaderContext,
.flashDriver = &g_flashDriverInterface,
.aesDriver = &g_aesInterface };

//! @}

And that first entry points at the expected function as verified with the Disassembly window:

bootloader_user_entry:
00000d2d: push {r7, lr}
00000d2f: sub sp, #8
00000d31: add r7, sp, #0
00000d33: str r0, [r7, #4]
00000d35: bl 0x5cc <Reset_Handler>

However, here is the kicker.  As shown below, I am heading right back where I started when I reset the system.  The MCU will reset, jump through its vector, run its inits, and direct boot back into my application.

void bootloader_user_entry(void *arg)
{
#if BL_TARGET_ROM || BL_TARGET_FPGA

// For ROM targets, we set the RCM_FM bits to force the ROM to run out of
// reset, then perform a reset. This provides a guaranteed clean system.
RCM_BWR_FM_FORCEROM(RCM, 0x3);
NVIC_SystemReset();

#elif BL_TARGET_FLASH

// For flash-resident configurations, just call the reset handler as the entry point.
Reset_Handler();

#elif !BL_TARGET_RAM
#error "Undefined target type"
#endif // BL_TARGET_ROM || BL_TARGET_FPGA
}


If I understand the way all of this works, we do want to reset, to reboot into the flash loader, to wipe out memory that was previously used by my application, but how does the freshly booted boot loader know that this time things are different and we want to skip the direct boot and perform a flash update? 

The hardware in my system does not have a signal it can put into a GPIO to indicate it wants to program which seems like a potential approach.  Without the hardware input, is this a mode that is dependent on receiving port input before a delay has timed out?  Are there other good options?

0 Kudos
5 Replies

1,020 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Don Willey,

    Please let me know what the kinetis chip you are using, please tell me the chip part number, I need to check whether it has the ROM Bootloade or not.

   Please also let me know what the bootloader your are using? Uart or others?

Waiting for your reply!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,020 Views
donwilley
Contributor II

Several.

MKL16Z128VLH4

MKL16Z128VFT4

MKL16Z32VFT4

MKL10Z64VLF7

From NXP documentation I have seen, none of these have a ROM bootloader.

0 Kudos

1,020 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Don,

   Thank you for your updated information.

   Yes, MKL16 don't have the ROM bootloader, so you need to use the flash bootloader.

   But don't worry, you can refer to our KL25 kboot flash bootloader code, please download the KBOOT2.0 from this link:

NXP_Kinetis_Bootloader_2.0.0 package

You can find the KL25 kboot flash bootloader code from folder:

NXP_Kinetis_Bootloader_2_0_0\targets\MKL25Z4

Then refer to Kinetis Bootloader v2.0.0 Reference Manual.pdf in folder: NXP_Kinetis_Bootloader_2_0_0\doc

Chapter 10 Kinetis bootloader porting

This post also for your reference:

How to make MKL26Z128 be recognized by KBOOT Flash Tool Utility? 

Please refer to the above material at first, if you still have questions about it, please kindly let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,020 Views
donwilley
Contributor II

Thanks for researching and giving a prompt reply to my questions.

I am pretty familiar with the material at the first link, but will dig in and see what might be applicable in the other two links.

0 Kudos

1,020 Views
kerryzhou
NXP TechSupport
NXP TechSupport

You are welcome.

 After you porting it, if you still have problems, just let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos