Dummy audio codec -  play & record on i.MX8MM

Document created by MaxTsai Employee on Jul 4, 2019Last modified by MaxTsai Employee on Jul 8, 2019
Version 3Show Document
  • View in full screen mode

Several customers met problem on audio codec porting. In order to figure out cpu dai setting problem or codec dai problem. Create the dummy codec for test purpose. 

 

What this dummy codec can do

This dummy codec can play up to 8 channels and record up to 6 channels.

Connect SAI1 TX data pin with SAI1 RX data pin for loopback test.

 

Environment

Verified with i.MX8MM EVK 

Based on Linux BSP L4.14.78

 

Files

Kernel patch

0001-multiple-channels-dummy-audio-codec

0002-Add-capture-for-multiple-channels

User space setting

/etc/asound.conf

/usr/share/alsa/cards/aliases.con

/usr/share/alsa/cards/DUMMY.conf

Audio test content

PCM_48_16_8_160000_1_29_jazzshort.wav

 

 

The alsa command for loopback test with multiple channels 

aplay -D surround51:CARD=dummyaudio PCM_48_16_8_160000_1_29_jazzshort.wav | arecord -D surround51:CARD=dummyaudio --disable-channels --disable-format --disable-resample -f S16_LE -r 48000 -c 6 -d 5 -v test.wav

2 people found this helpful

Outcomes