Example S32K144 FlexCAN0 RXFIFO DMA nonSDK S32DS13

Document created by Petr Stancik Employee on Sep 4, 2017Last modified by Adrian Puga Candelario on Mar 6, 2020
Version 5Show Document
  • View in full screen mode

********************************************************************************
Detailed Description:

Configures the FlexCAN 0 to transmit and receive message into RXFIFO.
LOOPBACK mode is enabled.
Two IDs are set into RXFIFO ID table.
DMA is configured to read the message from RXFIFO.
Within DMA major interrupt the new message is send according to
which Identifier Acceptance Filter was hit.

------------------------------------------------------------------------------
 Test HW:         S32K144 EVB-Q100
 MCU:             PS32K144HFVLL 0N77P
 Fsys:            160MHz
 Debugger:        Lauterbach
 Target:          internal_FLASH

********************************************************************************
Revision History:
1.0     Sep-4-2017     Petr Stancik    Initial Version
*******************************************************************************

8 people found this helpful

Outcomes