Demo
This demo shows the wide voltage operating range of the AXPnT Translator family.
An onboard oscillator provides a low frequency clock to drive the input channel. LEDs indicate the signal on the input and output side of the translator. Two dials allow the user to independently set the input and output voltage rails.
This demo visually shows how logic translators operate and that the AXPnT family has the widest operating range of current translators
Features:
_______________________________________________________________________________________________________
Featured NXP Products:
_______________________________________________________________________________________________________
SP02