How to use EzPort module

Document created by Lin Lu Employee on Sep 14, 2014Last modified by Lin Lu Employee on Sep 15, 2014
Version 6Show Document
  • View in full screen mode

Overview

     This document describes how to use ezport module on TWR-K22F120M,  and the usage of ezport on other platforms  is similar.

     The EzPort module is a serial flash programming interface that enables In-System Programming (ISP) of flash memory contents in a 32-bit general-purpose microcontroller.

     The block diagram of EzPort module is as follows:

bd.jpg

Hardware environments

  • TWR-K60D100M
  • TWR-K22F120M
  • TWR-SER
  • Primary and Secondary Tower boards

     Because the EzPort module is a serial flash programming interface that is compatible with a subset of the SPI format. TWR-K60D100M is used as a SPI master and TWR-K22F120M is used as a slave. The flash memory contents of TWR-K22F120M can be read/erased/programmed from TWR-K60D100M.

     Connect the TWR-K60D100M and TWR-SER by two tower boards, the execution result will be outputed by uart.

 

Step 1TWR-K22F120M enters into EzPort mode

Hardware setup: 

     If the TWR-K22F120M wants to enter EzPort mode, the EZP_CS pin should be asserted and then reset pin is asserted.

TWR-K60D100M                         TWR-K22F120M

PTC6(J11 A71)                           EZP_CS(J31 Pin9)

 

Software setup:

  1. Open the project “ezport_test_kinetis”;
  2. Define the MACRO “ENTER_EZPORT_MODULE” in hal_config.h;
  3. Build and download the program into TWR-K60D100M, run it, then EZP_CS pin of TWR-K22F120M will be asserted.
  4. Then power-on the TWR-K22F120M. The TWR-K22F120M will enter into EzPort mode.

 

Step 2: Use EzPort to read/erase/program the flash

Hardware setup:

TWR-K60D100M                         TWR-K22F120M

PTD0(J11 B63)                            EZP_CS(J31 Pin9)

PTD1(J11 B64)                            EZP_CLK(J31 Pin4)

PTD2(J11 A76)                            EZP_DI(J31 Pin8)

PTD3(J11 A77)                            EZP_DO(J31 Pin6)

GND(J11 B65)                             GND(J31 Pin5)

Note: TWR-K60D100M and TWR-K22F120M should have common ground.

Software setup:

  1. Open the project “ezport_test_kinetis”;
  2. Undefine the MACRO “ENTER_EZPORT_MODULE” in hal_config.h, then EzPort test codes will be enabled;
  3. Build and download the program into TWR-K60D100M, run it, then the flash memory contents of TWR-K22F120M can be read/erased/programmed from TWR-K60D100M, the execution result will output to the console by uart.

Attachments

Outcomes