MPC5200 Codewarrior version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5200 Codewarrior version

1,227 Views
trizio
Contributor I

I have to modify an old application based on an MPC5200 (not an MPC5200B)  processor using an emulator. What is the right version of  Codewarrior? What emulator can I use? In the past I have used an Parallel WireTap for PPC but now I have not the parallel port (I am using a new laptop) and I have an Slingshot usb emulator, is this compatible with the codewarrior?  

Tank you for your help. 

Labels (1)
0 Kudos
1 Reply

389 Views
stanish
NXP Employee
NXP Employee

Hello trizio,

 

MPC5200 is supported by the recent version of CodeWarrior MGT v9.2 (you can download Evaluation version here).

I'm affaid Slingshot usb interface is not supported.

List of supported interfaces and v9.2 release notes attached for your convenience.

 

Stanish 

Release_Notes_MGT_R9.2.txt

CW_9.2_Remote_Connection_List.jpg

Message Edited by t.dowe on 2009-10-01 03:22 PM
0 Kudos