解決済! 解決策の投稿を見る。
Hi
Here is code to configure a 2s watchdog timeout
CWCR = (CWE | WATCHDOG_2_SEC | CWTA | CWTAVA | CWTIF);
fnSetIntHandler(SW_WD_VECTOR, (unsigned char *)_sw_wdog_timeout);
IC_ICR_0_8 = (INTERRUPT_LEVEL_7 | INTERRUPT_PRIORITY_7);
IC_IMRL_0 &= ~(SW_WDG_PIF_INT_L | MASK_ALL_INT);
The handling routine is
static __interrupt__ void _sw_wdog_timeout(void)
{
RESET_RCR = SOFT_RST; // command a soft reset of the board
}
Note that the watchdog should best be given highest (NMI) priority so that it can fire when another interrupt routine fail.
It is however not fool-proof since it relies on the watchdog interrupt handler being able to run (which is not 100% guarantied) - see http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=1051&query.id=148409#...
The Backup Watchdog Timer in other V2 MCU parts (like Kirin3) is much improved. See http://www.utasker.com/forum/index.php?topic=505.0
Regards
Mark
www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M521X, M521XX, M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."
I'm running the InterNiche stack using the M52233Demo board also.
Same issue here. It doesn't work!!!!!!!!!
/**Int_handlers.c **/
__interrupt__ void wdtISR( void )
{
MCF_SCM_CWCR |=MCF_SCM_CWCR_CWTAVAL |MCF_SCM_CWCR_CWTIF ;
MCF_RCM_RCR |= MCF_RCM_RCR_SOFTRST; // Set software reset request bit.
}
/**Int_handlers.c **/
MCF_INTC0_ICR07=MCF_INTC_ICR_IL(7); //highest priority.
MCF_INTC0_IMRL &= ~( MCF_INTC_IMRL_INT_MASK1); //Using one other Interrupt.
MCF_INTC0_IMRL &= ~( MCF_INTC_IMRL_INT_MASK7); //Watchdog Interrupt.
MCF_SCM_CWCR = MCF_SCM_CWCR_CWE | // Enable WDT
MCF_SCM_CWCR_CWT_2_23 |
MCF_SCM_CWCR_CWTA | // Enable Transfer Ack.
MCF_SCM_CWCR_CWTAVAL ;
/***MCF52235_vectors.s**
vector48 .long _wdtISR
It never causes an interrupt at this vector.
The link says issued resolved. I say it isn't. Can anyone clear this up?
Thanks,
Terry
Hi terry,
just replace this line
MCF_INTC0_ICR07=MCF_INTC_ICR_IL(7); //highest priority.
to
MCF_INTC0_ICR08=MCF_INTC_ICR_IL(7); //highest priority.
Hey Abhijit,
Thanks for the quick reply. It gave me some focus on what to look for.
The only reference to Control registers concerning the Watchdog was the one below.
It wasn't very clear in this data sheet.
From the Data Sheet MCF52235RM.pdf Section 13-10..
CWRI
Core watchdog interrupt select.
0 If a time-out occurs, the CWT generates an interrupt to the processor core. The interrupt level for the CWT is
programmed in the interrupt control register 7 (ICR7) of INTC0.
Same code from me before but I hardcoded the ICR08 = 0x3F;
Here is what worked for me.......
MCF_SCM_CWCR = MCF_SCM_CWCR_CWE
| // Enable WDT
MCF_SCM_CWCR_CWT_2_23 |
MCF_SCM_CWCR_CWTA | // Enable Transfer Ack.
MCF_SCM_CWCR_CWTAVAL ;
MCF_INTC0_ICR08 |= 0x3F; //highest priority.
MCF_INTC0_IMRL &= ~( MCF_INTC_IMRL_INT_MASK8); //Watchdog Interrupt.
I was trying to fix the last couple lines. I hit the tab key which sent before I wanted to.......
Here is a cleaned up version.........
MCF_SCM_CWCR = MCF_SCM_CWCR_CWE
| MCF_SCM_CWCR_CWT_2_23
| MCF_SCM_CWCR_CWTA
| MCF_SCM_CWCR_CWTAVAL
| MCF_SCM_CWCR_CWTIF;
MCF_INTC0_ICR08 |= 0x3F; //highest priority.
MCF_INTC0_IMRL &= ~( MCF_INTC_IMRL_INT_MASK8); //Watchdog Interrupt.
MCF_INTC0_IMRL &= ~( MCF_INTC_IMRL_MASKALL); //Enable.
Thanks again Abhijit.......
Hi terry,
The configuration is looking fine but might be still remains something.
I'm not a expert but still i can give some ways to approch d task.
U can try without InterNiche.just create new project which include this
watch dog releted configuration.
Finally 1 question is remains dat how u test it???
In my case i made a basic timer who clear the releted register
MCF_SCM_CWSR = 0x55;
MCF_SCM_CWSR = 0xAA;
when i commented dat part i.e not clearing this then ISR is callled from vector48.
Hey Abhijit,
What helped me out the most was using a baseline Processor Expert project with having only a watchdog (no Internice). This showed me the correct values for all registers and vectors. The datasheet was just not clear enough.
I tested by setting a breakpoint at the interrupt vector routine and not writing the 0x55 & 0xAA to the CWSR.
It took about 20 seconds for the interrupt to engage. It works!
Thanks again,
TT
Hi
Here is code to configure a 2s watchdog timeout
CWCR = (CWE | WATCHDOG_2_SEC | CWTA | CWTAVA | CWTIF);
fnSetIntHandler(SW_WD_VECTOR, (unsigned char *)_sw_wdog_timeout);
IC_ICR_0_8 = (INTERRUPT_LEVEL_7 | INTERRUPT_PRIORITY_7);
IC_IMRL_0 &= ~(SW_WDG_PIF_INT_L | MASK_ALL_INT);
The handling routine is
static __interrupt__ void _sw_wdog_timeout(void)
{
RESET_RCR = SOFT_RST; // command a soft reset of the board
}
Note that the watchdog should best be given highest (NMI) priority so that it can fire when another interrupt routine fail.
It is however not fool-proof since it relies on the watchdog interrupt handler being able to run (which is not 100% guarantied) - see http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=1051&query.id=148409#...
The Backup Watchdog Timer in other V2 MCU parts (like Kirin3) is much improved. See http://www.utasker.com/forum/index.php?topic=505.0
Regards
Mark
www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M521X, M521XX, M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."