Hi there!
Complete newbie here. I just wanted to ask if SOF is already built in the board? I can access the aplay and amixer parameters within the board(via simple serial connection). I am trying to build an SOF environment in a Linux OS since the sof would be a more updated version. Trying to add additional audio modules to be integrated in the board. Any other resources available besides the SOF website? Thanks!
Hi Hasnain
I am afraid it is not integrated, Linux documentation Linux 5.4.3_1.0.0 Documentation
i.MX Software | NXP
describes what is integrated in nxp bsps.
One can try to follow Porting Guide included in linux documentation and
Build SOF from scratch — SOF Project 0.1 documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I have been following the same porting guide from SOF. But nevertheless thank you for your response!