IMX8MM - digital mic PDM input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MM - digital mic PDM input

1,252 Views
shai_b
Senior Contributor II

Dear team,

My customer has the following inquiry about PDM interface on IMX8MM, They need to connect a microphone that outputs PDM. They think they need to change the MCLK & DATA to one the SAI5 inputs, can you advise if this the correct way to interface with MIC.

for the MIC datasheet please refer https://www.mouser.co.il/datasheet/2/218/knowles_corporation_know-s-a0002305576-1-1736216.pdf  

Please find attached pic how they plan to connect it and advise us back.

Thanks in advance 

Kind regards,

shai.b@telsys.co.il

Labels (1)
Tags (2)
0 Kudos
1 Reply

1,210 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shai

I believe connections on picture are correct, note "SAI5 inputs"

are just pads name, input should be provided to pdm module,

for example PDM_CLK is muxed on SAI5_RXC pad.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos