I.Mx8mmini :LIBUSB_ERROR_TIMEOUT ] SDPU: write -f imx-boot-imx8mmevk-s

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.Mx8mmini :LIBUSB_ERROR_TIMEOUT ] SDPU: write -f imx-boot-imx8mmevk-s

4,142 Views
santhosh2
Contributor IV

Hi,

We are flashing our new i.mx8mmini PCB board and we are getting the error as below while flashing
---------------------------------------------------------------------------------------------------------
Success 0    Failure 1                                                        
                                                                               
1:13   2/ 3   [HID(W):LIBUSB_ERROR_TIMEOUT ] SDPU: write -f imx-boot-imx8mmevk-s
-----------------------------------------------------------------------------------------------------------
debug port trace Log is attached and uuu error screen shot is also attached for your quick reference 
Kindly let us know what may be the root cause of the above said error
LIBUSB_ERROR_TIMEOUT.png
0 Kudos
1 Reply

3,854 Views
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

one can look at answer on

Flashing iMX8MM-EVK using UUU Tool on Ubuntu 

issue with flashing Universal update utility for iMX8MQ · Issue #91 · NXPmicro/mfgtools · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos