Recording of audio is not happening

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recording of audio is not happening

788 Views
dhanushvenugopa
Contributor I

Hi,

I am using IMX6ULevk board with wm8960 codec,but when i want to record audio ,its not happening .

Please can i know what may be the problem and which part of the driver i need to check for mounting the mic and speaker of codec.

dts configuration:

sound: sound {
               compatible = "fsl,imx6ul-evk-wm8960",
               "fsl,imx-audio-wm8960";
                model = "wm8960-audio";
                cpu-dai = <&sai2>;
               audio-codec = <&codec>;
               asrc-controller = <&asrc>;
               codec-master;
               gpr = <&gpr 4 0x100000 0x100000>;
   audio-routing =
               "Headphone Jack", "HP_L",
               "Headphone Jack", "HP_R",
               "Ext Spk", "SPK_LP",
               "Ext Spk", "SPK_LN",
               "Ext Spk", "SPK_RP",
               "Ext Spk", "SPK_RP",

               "LINPUT2", "Mic Jack",
               "LINPUT3", "Mic Jack",
               "RINPUT1", "Main MIC",
               "RINPUT2", "Main MIC",
               "Mic Jack", "MICB",
               "Main MIC", "MICB",
               "CPU-Playback", "ASRC-Playback",
               "Playback", "CPU-Playback",
               "ASRC-Capture", "CPU-Capture",
               "CPU-Capture", "Capture";
};

Labels (1)
0 Kudos
1 Reply

658 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dhanush

one can try steps given in sect.7.3.5 Audio recording attached Linux Guide

with Demo Images on i.MX Software and Development Tools | NXP 

Linux Binary Demo Files - i.MX 6UltraLite, i.MX 6ULL, i.MX 7Dual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos