Interface an external RAM with i.MX RT 1062

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interface an external RAM with i.MX RT 1062

1,035 Views
biccius
Contributor I

Hello everybody,

I was asked to make a project which requires the fastest access possible to a RAM (write and read).

I am still in a study phase and at the moment it seems to me that the SEMC interface on a i.mx rt 1062 allows to do this.


Has anyone already had experience of this and if so, what type or model of RAM have you used and with what performance?


Thanks

Labels (1)
0 Kudos
1 Reply

841 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Use the following app note:

“i.MX RT Series Performance Optimization”

 

https://www.nxp.com/docs/en/application-note/AN12437.pdf 

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos