Is it possible to use the OM-SE050ARD kit together with non-NXP boards?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to use the OM-SE050ARD kit together with non-NXP boards?

1,202 Views
jordijofrenxp
NXP Employee
NXP Employee

Yes, it is. On the one hand, if you are using an Arduino-compatible MCU board, you can connect it using the Arduino connectors. On the other hand, if you are using a non-Arduino board, you can connect it using the external I2C connector

Labels (1)
Tags (1)
0 Kudos
0 Replies