Hi,
Hi,
Yes, you could implement a USB-Serial for secondary Debug option, but it is required to first boot the system to load the USB drivers/classes, so, it won’t be available on early boot stages.
Regarding activity of other pins during the boot, they are the boot selector GPIOs that may select entering to serial downloader mode, which could be implemented by USB or by UART. Please refer to Figure 6-1 “Boot flow” of the i.MX8M Mini Reference Manual.
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------
HI Carlos,
Can you please clarify that there aren't any UART prints made from within the on-chip boot ROM.
i.e. all UART activities are explicitly activated in uboot, correct?