DEMO9S12PFAME: Unexpected "ILLEGAL_BP" Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEMO9S12PFAME: Unexpected "ILLEGAL_BP" Error

3,519 Views
rajpanse
Contributor I

Hi,

I am facing a problem/difficulty while building a simple application using demo-board "DEMO9S12PFAME" for MC9S12P128. I have worked with Freescale 16-bit automotive MCUs in the past and I strongly suspect that the current problem may not be trivial. Would highly appreciate your assistance on this..

For you to be able to replicate the problem at your end on the same demo-board, I have described below a step-by-step procedure and have also attached the relevant project files:

The exact problem: Run-time failure. More specifically, CodeWarrior's True-Time Simulator reports an “illegal breakpoint” immediately after the attached code starts execution on the target device.

------------------------------------
* Hardware environment: DEMO9S12PFAME (Demo-board for MC9S12P128)

* Programming environment: CodeWarrior v4.7

* OS: Windows XP

Pls follow the following four steps to replicate the problem for the above-mentioned environment:
------------------------------------
Step 1: Create a new project using the following CodeWarrior options:
* Derivative: MC9S12P128
* Language: C
* Project set up for PC-lint (TM): No
* Level of startup code: ANSI startup code
* Floating point format: IEEE32 for both double and float
* Memory model: Small
* Connections: SofTec HCS12

Step 2: Copy the contents of the attached main.c into the main.c file for the project. Choose the “debug” button from CodeWarrior IDE for downloading code on the target.

Step 3: While downloading the code, choose the following option in true-time simulator & Real-time debugger:
* HW model - Code: DEMO9S12PFAME

Step 4: Click the "run" button. The device raises an “illegal breakpoint” error.
------------------------------------

Would appreciate your support.

Thanks.
Raj Panse

-----------------------------------------------------------------

P.S.: A description for the attachments is as follows:

1. Installed Plugins.TXT: Contains the CodeWarrior version details
2. Report.zip: Contains (zipped) project files. This project fails in the run-time by producing the reported problem.
3. main.c A copy of the main.c file from the project "Report".

-----------------------------------------------------------------

 

main4.c

Installed_Plugins5.txt

Report1.zip

Message Edited by t.dowe on 2009-08-28 03:32 PM
Labels (1)
0 Kudos
5 Replies

663 Views
Deadstar
Contributor I
Hey,

From my experience this is normally caused by not specifying an interrupt service routing in the interrupt vector table. I am not sure if your code is triggering interrupts but I have noticed you haven't specified any in your PRM linker file.

Colin
0 Kudos

663 Views
rajpanse
Contributor I
Thanks Colin.

Yes,  it is true that "ILLEGAL_BP" normally pops up when an interrupt is specified but the corresponding ISR is not specified in your code.

However, as you've noticed rightly, my code does not specify any interrupt. Therefore, it is quite surprising for me to see this error..

Raj
P.S.: The same code works flawlessly on MC9S12XS128 platform!

0 Kudos

663 Views
kef
Specialist I
Try commenting EnableInterrupt. Maybe /IRQ pin is pulled low? Then you should disable IRQ interrupt before unmasking all I-interrupts.
0 Kudos

663 Views
rajpanse
Contributor I
Got the issue solved!

Was using CodeWarrior 4.7 before and was receiving the error repeatedly. Just happened to patch it (4.7.1) from the web and everything started working :smileyhappy:

Seems that unpatched CodeWarrior 4.7 does not compile it right for the S12P family..

Raj
0 Kudos

663 Views
K_p
Contributor I

Have similliar kind of problems, but i have CW 5.9.

 

Code crashes during PE low level int and when i use debugger to "reset" program and press start/continue again code will work as it should be. what could cause that Illegal break point?

 

One noticetable feature is, that when i send a message to can bus, when i run this code without debugger, it wake ups the device.

 

At this version it crashes at PWM-init, when it executes HWEnDi there, but when I dissable PWM from the project the bug moves into next bean (in this case AD-module).

 

Any ideas, or is this a PE-bug in S12P?

 

current PE low level init code:

void PE_low_level_init(void)
{
  /* Common initialization of the CPU registers */
  /* WOMM: WOMM1=0 */

  clrReg8Bits(WOMM, 2);               


  /* RDRM: RDRM5=0,RDRM4=0,RDRM3=0,RDRM2=0,RDRM1=0,RDRM0=0 */

  clrReg8Bits(RDRM, 63);                


  /* TSCR1: TEN=0,TSWAI=0,TSFRZ=0,TFFCA=0,PRNT=1,??=0,??=0,??=0 */

  setReg8(TSCR1, 8);                    


  /* OCPD: OCPD7=1,OCPD6=1,OCPD5=1,OCPD4=1,OCPD3=1,OCPD2=1,OCPD1=1,OCPD0=1 */

  setReg8(OCPD, 255);                   


  /* PACTL: CLK1=0,CLK0=0 */

  clrReg8Bits(PACTL, 12);         

      
  /* OC7M: OC7M0=0 */

  clrReg8Bits(OC7M, 1);                 

 

  /* TIOS: IOS7=1,IOS0=1 */

  setReg8Bits(TIOS, 129);               


  /* TCTL2: OM0=0,OL0=0 */

  clrReg8Bits(TCTL2, 3);                


  /* TTOV: TOV7=0,TOV0=0 */

  clrReg8Bits(TTOV, 129);               


  /* TCTL1: OM7=0,OL7=0 */

  clrReg8Bits(TCTL1, 192);              


  /* TSCR2: TOI=0,TCRE=1 */

  clrSetReg8Bits(TSCR2, 128, 8);        


  /* TFLG1: C7F=1,C6F=1,C5F=1,C4F=1,C3F=1,C2F=1,C1F=1,C0F=1 */

  setReg8(TFLG1, 255);                  


  /* TIE: C0I=1 */

  setReg8Bits(TIE, 1);                  


  /* PTPSR: PTPS7=0,PTPS6=0,PTPS5=0,PTPS4=0,PTPS3=0,PTPS2=0,PTPS1=0,PTPS0=0 */

  setReg8(PTPSR, 0);                    

 

  /* PWME: ??=0,??=0,PWME5=0,PWME4=0,PWME3=0,PWME2=0,PWME1=0,PWME0=0 */

  setReg8(PWME, 0);                     


  /* PTTRR: PTTRR0=0 */

  clrReg8Bits(PTTRR, 1);                


  /* PWMCTL: CON01=0,PSWAI=0,PFRZ=0 */

  clrReg8Bits(PWMCTL, 28);              

 

  /* PWMCAE: CAE0=0 */

  clrReg8Bits(PWMCAE, 1);               


  /* PWMPOL: PPOL0=0 */

  clrReg8Bits(PWMPOL, 1);               


  /* PTP: PTP0=0 */

  clrReg8Bits(PTP, 1);                  


  /* DDRP: DDRP0=1 */

  setReg8Bits(DDRP, 1);                 


  /* ATDDIENL: IEN1=0,IEN0=0 */

  clrReg8Bits(ATDDIENL, 3);             


  /* PORTA: PA3=0,PA0=0 */

  clrReg8Bits(PORTA, 9);                


  /* PUCR: PUPAE=0 */

  clrReg8Bits(PUCR, 1);                 


  /* DDRA: DDRA3=1,DDRA0=1 */

  setReg8Bits(DDRA, 9);                 


  /* CPMUINT: LOCKIE=0,OSCIE=0 */

  clrReg8Bits(CPMUINT, 18);             


  /* CPMULVCTL: LVIE=0 */

  clrReg8Bits(CPMULVCTL, 2);            


  /* RDRIV: RDPE=0,RDPB=0,RDPA=0 */

  clrReg8Bits(RDRIV, 19);               


  /* RDRJ: RDRJ7=0,RDRJ6=0,RDRJ2=0,RDRJ1=0,RDRJ0=0 */

  clrReg8Bits(RDRJ, 199);               


  /* RDRP: RDRP7=0,RDRP5=0,RDRP4=0,RDRP3=0,RDRP2=0,RDRP1=0,RDRP0=0 */

  clrReg8Bits(RDRP, 191);               


  /* RDRS: RDRS3=0,RDRS2=0,RDRS1=0,RDRS0=0 */

  clrReg8Bits(RDRS, 15);                


  /* RDRT: RDRT7=0,RDRT6=0,RDRT5=0,RDRT4=0,RDRT3=0,RDRT2=0,RDRT1=0,RDRT0=0 */

  setReg8(RDRT, 0);                     


  /* RDR0AD: RDR0AD1=0,RDR0AD0=0 */

  clrReg8Bits(RDR0AD, 3);               


  /* RDR1AD: RDR1AD7=0,RDR1AD6=0,RDR1AD5=0,RDR1AD4=0,RDR1AD3=0,RDR1AD2=0,RDR1AD1=0,RDR1AD0=0 */

  setReg8(RDR1AD, 0);                   


  /* IRQCR: IRQEN=0 */

  clrReg8Bits(IRQCR, 64);               


  /* ### MC9S12P128_80 "Cpu" init code ... */

  /* ### Init_MSCAN "CAN1" init code ... */
  /* ### Call "CAN1_Init();" init method in a user code, i.e. in the main code */
  /* ### Note:   To enable automatic calling of the "CAN1" init code here must be
                 set the property Call Init in CPU init.code to 'yes'  */
  /* ### TimerInt "TI1" init code ... */
  /* TC0: BIT15=0,BIT14=0,BIT13=0,BIT12=0,BIT11=1,BIT10=0,BIT9=0,BIT8=1,BIT7=1,BIT6=1,BIT5=0,BIT4=0,BIT3=0,BIT2=1,BIT1=0,BIT0=0 */

  setReg16(TC0, 2500);                 /* Store given value to the compare register */

 

  /* TC7: BIT15=0,BIT14=0,BIT13=0,BIT12=0,BIT11=1,BIT10=0,BIT9=0,BIT8=1,BIT7=1,BIT6=1,BIT5=0,BIT4=0,BIT3=0,BIT2=1,BIT1=0,BIT0=0 */

  setReg16(TC7, 2500);                 /* Store given value to the modulo register */


  /* ###  WatchDog "WDog1" init code ... */
  /* CPMUPROT: ??=0,??=0,??=1,??=0,??=0,??=1,??=1,PROT=0 */

  setReg8(CPMUPROT, 38);               /* Disable protection of clock-source register */


  /* CPMUCLKS: PCE=0,COPOSCSEL=0 */

  clrReg8Bits(CPMUCLKS, 5);             


  /* CPMUPROT: ??=0,??=0,??=0,??=0,??=0,??=0,??=0,PROT=0 */
  setReg8(CPMUPROT, 0);                /* Re-Enable protection of clock-source register */


  /* CPMUCOP: WCOP=0,CR2=0,CR1=0,CR0=1 */

  clrSetReg8Bits(CPMUCOP, 134, 1);      

 

  /* ### Programable pulse generation "PWM6" init code ... */

  PWM6_Init();


  /* ###  "AD1" init code ... */

  AD1_Init();


  /* ### BitIO "Bit1" init code ... */
  Shadow_A &= (byte)~1;                /* Initialize pin shadow variable bit */


  /* ###  IntFLASH "IFsh1" init code ... */
  IFsh1_Init();


  /* ### BitIO "Bit2" init code ... */
  Shadow_A &= (byte)~8;                /* Initialize pin shadow variable bit */


 /* Common peripheral initialization - ENABLE */
  /* TSCR1: TEN=1 */
  setReg8Bits(TSCR1, 128);              
  __DI();                              /* Disable interrupts */

 

 

0 Kudos