imx8qm mek android P9 AUTO 使用板载HDMI_TX显示

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qm mek android P9 AUTO 使用板载HDMI_TX显示

976 Views
dhty2015
Contributor II

大家好:

我现在使用的是imx8qm mek 板子,当前的android P9 AUTO 版本只能编译出lvds-hdmi显示的版本,请问现在 android P9 AUTO版本代码已经支持板载的HDMI_TX显示吗?如果有,需要怎么配置?谢谢~

hi everyone:

I am using the imx8qm mek board now, the current android P9 AUTO version can only compile the version shown by lvds-hdmi, may I ask whether the code of android P9 AUTO version already supports the display of HDMI_TX on the board?If yes, how do I configure it?thank you~

0 Kudos
1 Reply

787 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Yuelin,

   i.MX8QM is still in pre-production now, I can only give you some guidance on your questions. see below, please!

---------------------

   You will need to re-compile device tree with fsl-imx8qm-mek-hdmi.dts, then check if hdmi driver has been selected in linux kernel, if not, select it , please! then re-compile kernel, and try.

--------------------

Hope above information can help you!

Have a nice day!

BR,

Weidong

0 Kudos