LOGO : The logo _flag =0
In: serial
Out: serial
Err: serial
Found PFUZE100 deviceid=10,revid=11
000f: 70 05 p.
ch_per = 87 %
MIT ZYNQ reboot
check_and_clean: reg 0, flag_set 0
Fastboot: Normal
flash target is SATA
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: ncq stag pm led clo only pmp pio slum part
SATA Device Info:
S/N: 50026B724114B0EF
Product model number: KINGSTON SMS200S330G
Firmware version: 524ABBF0
Capacity: 58626288 sectors
Net: Phy not found
FEC [PRIME]
Warning: failed to set MAC address
Normal Boot
Hit any key to stop autoboot: 0
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: ncq stag pm led clo only pmp pio slum part
SATA Device Info:
S/N: 50026B724114B0EF
Product model number: KINGSTON SMS200S330G
Firmware version: 524ABBF0
Capacity: 58626288 sectors
reading uramdisk.img
727254 bytes read in 13 ms (53.4 MiB/s)
reading uImage
9781728 bytes read in 88 ms (106 MiB/s)
reading imx6q-sabresd-ldo.dtb
52452 bytes read in 8 ms (6.3 MiB/s)
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux-4.9.17-03714-g7e8c41b
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 9781664 Bytes = 9.3 MiB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
Wrong Ramdisk Image Format
Ramdisk image is corrupt or invalid
=>
Hello Mahesh Bhagoji,
Porting a Kernel version is not a trivial task as there are many variables. There is already a 4.9 official BSP and community BSP for the i.MX6 and i.MX7 that may be of help if you want to use one of those Kernels instead of porting it by yourself.
Regards,