Rotate mipi-dsi display to landscape mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Rotate mipi-dsi display to landscape mode

2,001 Views
RuiBastos
Contributor II

hello,

I'm using a apalis-imx6 toradex custom board with mipi-dsi display. The default display orientation is portrait with 480x800 resolution.

mxc_sdc_fb fb@0: 480x800 h_sync,r,l: 8,8,8 v_sync,l,u: 8,2,10 pixclock=24796000 Hz

As you can see the default portrait orientation is working finealt text ,

but when I rotate to right using xrandr -o right the image do not fill all the screen.

01_landscape.jpg

and I want to use landscape mode all the time, since the display initialization.

someone can help me ?

thanks

Rui

Labels (2)
0 Kudos
1 Reply

1,610 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rui

one can check suggestions provided on

Best practice to rotate 90 degrees and flip screen for the Framebuffer - Toradex Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos