GPS Service was kickout while selinux is enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPS Service was kickout while selinux is enabled

1,242 Views
bensonwu
Contributor III

I am developing Android platform (Oreo) with imx6dl and imx6Q

Recently, I just add ublox GNSS driver (v3.5) from ublox on my platform and met a problem related to Selinux.

  • If OS was built with Selinux is enabled(enforced) , ublox driver tried to bind but failed continuously(kicked repeatedly) and the message is as below:

/****************************************************************************/

init: starting service 'ubx-gnss'...
init: property_set("init.svc.ubx-gnss", "running") OK!
init: property_set("ro.boottime.ubx-gnss", "964917483781") failed: property already set
init: Service 'ubx-gnss' (pid 1515) killed by signal 6
init: Sending signal 9 to service 'ubx-gnss' (pid 1515) process group...
init: Successfully killed process cgroup uid 0 pid 1515 in 0ms
init: property_set("init.svc.ubx-gnss", "restarting") OK!
init: Untracked pid 1518 exited with status 0
130|sabresd_6dq:/ # starinit: starting service 'ubx-gnss'...
init: property_set("init.svc.ubx-gnss", "running") OK!
init: property_set("ro.boottime.ubx-gnss", "969921627782") failed: property already set
init: Service 'ubx-gnss' (pid 1523) killed by signal 6
init: Sending signal 9 to service 'ubx-gnss' (pid 1523) process group...
init: Successfully killed process cgroup uid 0 pid 1523 in 0ms
init: property_set("init.svc.ubx-gnss", "restarting") OK!
init: Untracked pid 1526 killed by signal 13

................

/***************************************************************/

  • the result of getprop is as below:

[init.svc.ubx-gnss]: [restarting]

[ro.boottime.ubx-gnss]: [10671214334]

However, if I built OS with disable Selinux( add androidboot.selinux=permissive in bootarg ) then ublox driver can be attached successfully. and NMEA message can come out 

Logs:

/**************************************************************************/

init: starting service 'ubx-gnss'...
init: property_set("init.svc.ubx-gnss", "running") OK!
init: property_set("ro.boottime.ubx-gnss", "2643702243981") failed: property already set

/*************************************************************************/

getprop:

[init.svc.ubx-gnss]: [running]
[ro.boottime.ubx-gnss]: [10671214334]

There is no related AVC message . My GPS port is i2c-0 .

/*********************************************************/

# dmesg | grep avc
[ 11.278137] type=1400 audit(15.880:4): avc: granted { read } for pid=1 comm="init" name="ttymxc0" dev="tmpfs" ino=9581 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 15.640669] type=1400 audit(15.880:4): avc: granted { read } for pid=1 comm="init" name="ttymxc0" dev="tmpfs" ino=9581 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 15.679859] type=1400 audit(15.880:5): avc: granted { read open } for pid=1 comm="init" path="/dev/ttymxc0" dev="tmpfs" ino=9581 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 15.696924] type=1400 audit(15.880:5): avc: granted { read open } for pid=1 comm="init" path="/dev/ttymxc0" dev="tmpfs" ino=9581 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 15.714734] type=1400 audit(16.000:6): avc: granted { read } for pid=277 comm="init" name="ttymxc0" dev="tmpfs" ino=9581 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 15.732394] type=1400 audit(16.000:6): avc: granted { read } for pid=277 comm="init" name="ttymxc0" dev="tmpfs" ino=9581 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 15.748371] type=1400 audit(16.000:7): avc: granted { read open } for pid=277 comm="init" path="/dev/ttymxc0" dev="tmpfs" ino=9581 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 1020.549032] type=1400 audit(16.000:7): avc: granted { read open } for pid=277 comm="init" path="/dev/ttymxc0" dev="tmpfs" ino=9581 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file

/**************************************************************/

Further information in later experiment:

I try to build OS image with disable Selinux but I purposely enter the incorrect path for library , then I got the SAME error messages as the OS image with enabled Selinux.

/****************************************************************************/

init: starting service 'ubx-gnss'...
init: property_set("init.svc.ubx-gnss", "running") OK!
init: property_set("ro.boottime.ubx-gnss", "964917483781") failed: property already set
init: Service 'ubx-gnss' (pid 1515) killed by signal 6
init: Sending signal 9 to service 'ubx-gnss' (pid 1515) process group...
init: Successfully killed process cgroup uid 0 pid 1515 in 0ms
init: property_set("init.svc.ubx-gnss", "restarting") OK!
init: Untracked pid 1518 exited with status 0
130|sabresd_6dq:/ # starinit: starting service 'ubx-gnss'... 
init: property_set("init.svc.ubx-gnss", "running") OK!
init: property_set("ro.boottime.ubx-gnss", "969921627782") failed: property already set
init: Service 'ubx-gnss' (pid 1523) killed by signal 6
init: Sending signal 9 to service 'ubx-gnss' (pid 1523) process group...
init: Successfully killed process cgroup uid 0 pid 1523 in 0ms
init: property_set("init.svc.ubx-gnss", "restarting") OK!
init: Untracked pid 1526 killed by signal 13

................

/***************************************************************/

It seemed that I have permission issue to access shared library when Selinux is enabled. 

 Please give me some help if possible. Thank you!

Labels (1)
0 Kudos
2 Replies

910 Views
luwinbo
Contributor III

I will suggest to you that disabled your service first, and start it after boot_completed, just as follows, the system will give you enough message about permission, and then you just add the permission what it needs.

service ubx-gnss

      disabled

on property:sys.boot_completed=1
     bootchart stop

     start ubx-gnss

910 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Benson Wu,

I would recommend looking for insight on the Google Developer forums as permissions in newer Android versions are becoming more intricate.

There are a couple of threads in our communities regarding Selinux but not for Oreo, like the one below. So a dedicated Android forums may provide better information.

https://community.nxp.com/message/1065246?commentID=1065246#comment-1065246

My apologies for the inconvenience!

Regards,

0 Kudos