I am trying to play video in qtwebkit using gstreamer 1.0. I can see that gstreamer get called, plugins is loaded, src and sink is setup etc but then it just stops and no video is showed in the browser. I use the qt5 example browser to test it. I build Sumo yocto without wayland and x11. Is there anything specific that needs to be done to enable this combination? Video plays as it should with gst-play-1.0.
IMAGE_INSTALL_append += "\
packagegroup-imx-tools-audio \
imx-codec \
pulseaudio \
qtbase-plugins \
qtbase-tools \
qtdeclarative \
qtdeclarative-plugins \
qtdeclarative-tools \
qtdeclarative-qmlplugins \
qtmultimedia \
qtmultimedia-plugins \
qtmultimedia-qmlplugins \
qtsvg \
qtsvg-plugins \
qtsensors \
qtimageformats-plugins \
qtsystems \
qtsystems-tools \
qtsystems-qmlplugins \
qtscript \
qt3d \
qt3d-qmlplugins \
qt3d-tools \
qtwebkit \
qtwebkit-examples-examples \
qtwebkit-qmlplugins \
qtgraphicaleffects-qmlplugins \
qtconnectivity-qmlplugins \
qtlocation-plugins \
qtlocation-qmlplugins \
gstreamer1.0-plugins-imx \
gstreamer1.0-plugins-imx-meta \
gstreamer1.0-plugins-bad \
gstreamer1.0-plugins-base \
gstreamer1.0-plugins-good \
packagegroup-fsl-gstreamer1.0 \
packagegroup-fsl-tools-testapps \
imx-vpu \
imx-test \
firmware-imx-vpu-imx6d \
"
DISTRO_FEATURES_remove = "X11 wayland"
DISTRO_FEATURES_append = "directfb"
PACKAGECONFIG_append_pn-qtmultimedia = " examples gstreamer"
PACKAGECONFIG_append_pn-qtdeclarative = " qtxmlpatterns"
PACKAGECONFIG_append_pn-qtbase = " linuxfb accessibility "
PACKAGECONFIG_remove_pn-gstreamer1.0-plugins-good = " gdk-pixbuf"
The logs ends with these lines. I'm not sure what the timed out at the end means or how to figure out what element/plugin is causing it.
0:00:10.851254563 3447 0x1711600 INFO basesrc gstbasesrc.c:1331:gst_base_src_do_seek:<appsrc0> seeking: bytes segment start=0, offset=0, stop=-1, rate=1.000000, applied_rate=1.000000, flags=0x00, time=0, base=0, position 0, duration -1
0:00:10.851607863 3447 0x1711600 INFO task gsttask.c:457:gst_task_set_lock: setting stream lock 0x19e0084 on task 0x19f8828
0:00:10.851728851 3447 0x1711600 INFO GST_PADS gstpad.c:6068:gst_pad_start_task:<appsrc0:src> created task 0x19f8828
0:00:10.852858077 3447 0x1711600 INFO GST_STATES gstelement.c:2467:gst_element_continue_state:<appsrc0> completed state change to PAUSED
0:00:10.853009062 3447 0x1711600 INFO GST_STATES gstelement.c:2372:_priv_gst_element_state_changed:<appsrc0> notifying about state-changed READY to PAUSED (VOID_PENDING pending)
0:00:10.853207043 3447 0x1711600 INFO GST_STATES gstbin.c:2945:gst_bin_change_state_func:<source> child 'appsrc0' changed state to 3(PAUSED) successfully
0:00:10.853313033 3447 0x19ace90 INFO GST_ELEMENT_PADS gstelement.c:915:gst_element_get_static_pad: no such pad 'sink' in element "appsrc0"
0:00:10.853469018 3447 0x1711600 INFO GST_STATES gstelement.c:2467:gst_element_continue_state:<source> completed state change to PAUSED
0:00:11.185429405 3447 0x19ace90 FIXME default gstutils.c:3902:gst_pad_create_stream_id_internal:<appsrc0:src> Creating random stream-id, consider implementing a deterministic way of creating a stream-id
0:00:11.185413074 3447 0x1711600 INFO GST_STATES gstelement.c:2372:_priv_gst_element_state_changed:<source> notifying about state-changed READY to PAUSED (VOID_PENDING pending)
0:00:11.185880696 3447 0x1711600 INFO GST_STATES gstbin.c:2080:gst_bin_get_state_func:<play> getting state
0:00:11.185991352 3447 0x1711600 INFO GST_STATES gstelement.c:2185:gst_element_get_state_func:<play> waiting for element to commit state
0:00:11.186134005 3447 0x1711600 INFO GST_STATES gstelement.c:2199:gst_element_get_state_func:<play> timed out
0:00:11.186456308 3447 0x19ace90 INFO GST_PADS gstpad.c:4167:gst_pad_peer_query:<typefind:src> pad has no peer
We are using the Sumo Yocto build from Congatec as we are using modules from them.
Qseven Computer-On-Modules - congatec AG
I expected that to include support for graphics acceleration. Was I wrong?
And secondly, running gstreamer stand alone seems to work with graphics acceleration, it it first with combination with qtwebkit that I don't get any output. Do NXP need to add anything to QT for it to work with imx6?
Hi Gustav
Congatec software is supported by Congatec tech support.
Technical Support - congatec AG
NXP supports only own BSPs described on
NXP software repository
Best regards
igor
Hi Gustav
for sumo nxp have only Linux L4.14.62_1.0.0_Beta:
Linux L4.14.62_1.0.0_Beta Documentation
one can try with latest GA official release Linux 4.9.88 (rocko)
Linux 4.9.88_2.0.0 BSP & Multimedia Codecs Documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------