Adding new working point - frequency in linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding new working point - frequency in linux

953 Views
mohamad-ahmad
Contributor III
Deciding what frequency within the CPUfreq policy should be used is achieved using "cpufreq governors".
Inside the CPUFreq we can find:
# ls /sys/devices/system/cpu/cpu1/cpufreq/
affected_cpus
related_cpus
scaling_max_freq
bios_limit
scaling_available_frequencies
scaling_min_freq
cpuinfo_cur_freq
scaling_available_governors
scaling_setspeed
cpuinfo_max_freq
scaling_cur_freq
stats
cpuinfo_min_freq
scaling_driver
cpuinfo_transition_latency
scaling_governor
scaling_available_frequencies shows all available frequencies, for example:
# cat scaling_available_frequencies
2997000 2664000 2331000 1998000
How can I add more frequency values?
Can anyone please help me to add additional intermediate frequency values?
Is that can be done in Linux config (kernel compilation) or in the cpufreq driver?
Regrads
Mohamad
0 Kudos
2 Replies

781 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mohamad,

Please review the documents mentioned on the following thread. You would need to add the desired frequencies to the board Device Tree.

https://community.nxp.com/message/962882?commentID=962882#comment-962882

I hope this helps!

Regards,

0 Kudos

781 Views
mohamad-ahmad
Contributor III

Hi Gusarambula,

The answer that exists in this thread is very helpful!

Thank you

0 Kudos