LS1046ARDB development board MINIPCIE interface used network card model?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046ARDB development board MINIPCIE interface used network card model?

389 Views
17319399281
Contributor I

We are using the LS1046A development board. We want to use the MINIPCIE interface above to realize wifi and bluetooth functions. Is there any recommended model

When the development board is designed, when the wifi function is tested, which interface is used?What type of network card.

The module needs to integrate both wifi and bluetooth functions. Wifi supports AP mode and bluetooth V4.2 or above

0 Kudos
1 Reply

313 Views
ufedor
NXP Employee
NXP Employee

The WNC DNXA-H1 was tested with the LS1046ARDB - please refer to:

https://www.nxp.com/docs/en/user-guide/IIoT_UG.pdf 

0 Kudos