MMZ25332BT1 failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMZ25332BT1 failure

534 Views
milos_milosavlj
Contributor I

Dear All,

I have a question about the MMZ25332BT1 power amplifier (PA) that we are using in our radios. Occasionally we see some PA failures that we are still not sure what they are caused by.

Basically we see a dropped current draw from the PA, reduced output power and the Pdet shows 0V (in normal operation the correct voltage is outputed from the Pdet). What can cause such a failure? On one of them we could see the 0V on the Pdet and the full output power. Since this is dual stage PA we assumed that maybe only one stage fails but still cant explain it.

Any comments will be highly appreciated.

Thanks

Milos

Labels (1)
  • RF

0 Kudos
1 Reply

415 Views
LPP
NXP Employee
NXP Employee

Power HBT is comprised from multiple fingers. Overstress may cause some fingers to fail in sequence. It can be seen as progressive degradation of the performance. Your observation of Pdet signal may be a sequence of a ‘fused’ signal runner (single or a small close group) that may disconnect the Pdet node from the other functional output fingers.

In many cases, poor grounding leads to oscillation failures. Maintaining a good interface between the transistor and the circuit is essential  to prevent oscillation related ruggedness failures. Typical RF board provides multiple vias along the active traces and all arownd the board to provide RF path between top/bottom ground layers.

The next two reasons are: poor thermal management and operating at high VSWR conditions (no load or short circuit).

Typically a fail will be accompanied by physical damage evident on the die itself which can be observed by microscopic inspection. If you would like analysis on the failed devices, they can be returned to NXP for continued assistance. Please, contact the distributor who sold you these parts to submit the request to NXP.

I hope you will find these information useful. If we can be of additional assistance, please let us know.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos