hi
how to flash hex file LPCXpresso 54114 eval board, i'm trying flash hex file with "Flash magic Tool" getting some Error "auto Boud" can you help me any other open source flashing tool.
Hi,
In order to use the Flash magic Tool for the LPCXpresso 54114 eval board, please check the following steps:
1. Unplug the USB cable (if attached).
2. Press and hold the ISP0 SW2 button.
3. Plug in a USB cable from a USB computer to the J7 (“Link”).
4. Release the SP0 SW2 button.
5. Open Flash magic Tool
6. Select the device and the COM port.
The COM Port depends on the Communications Port of your Computer's RS232. When you use this COM Port with FlashMagic – be sure that no other program is using it at this time.
You can check the COM port using the device manager >Ports (COM & LPT)
7. If you want to check if FlashMagic is working with your board use the "Read Device Signature" option:
If everything is ok you will see this window with your device ID on it.
I hope this helps,
Have a great day,
Soledad
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thanks very much
then next step what will do
Thanks
It's Working.