When boot up, the PAD_UART2_TXD is configured as TXD Pin of UART2. And I use UART2 to communicate with peripheral device. But I need to send one pulse through PAD_UART2_TXD then back to UART function. How should I do?
Hi Jason
seems one can write to iomux registers directly in application,
if this is linux this may be posted on kernel mail list:
Majordomo Lists at VGER.KERNEL.ORG
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------