Hi,
We are using LS1012AFRDM board and linux SDK (QorIQ-SDK-V2.0-20160527-yocto) installed on PC (Ubuntu 14.04) for development. Now for our custom board we want to configure MC34VR5100A1EP chip to provide different voltages. We want understand different I2C files used in LS1012AFRDM to configured MC34VR5100A1EP. So that we can modify the required configuration in uboot or kernel.
Regards
Minal
There is no driver for the MC34VR5100A1EP programming in kernel or u-boot in SDK 2.0-1703 or LSDK.
Usually external I2C tool is used for the MC34VR5100A1EP programming.
NXP SDK for i.mx contains drivers for PMIC using. See attached file.
Use this driver as example for the MC34VR5100A1EP programming.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pavel
Thanks for the information. I will check the attached driver file.
Thanks & Regards
Minal