CLKP/CLKN requirement of MIPI-CSI2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLKP/CLKN requirement of MIPI-CSI2

Jump to solution
1,605 Views
takayuki_ishii
Contributor IV

Hello community,

We have a question about CLKP/CLKN of MIPI-CSI2 of i.MX6Q.

While blanking area of input video, Does it must input MIPI clock continuously?

Or it must gated to input MIPI clock while blanking area?

Which type of clock control does i.MX6Q required?

Best regards,

Ishii.

Labels (1)
Tags (1)
0 Kudos
1 Solution
1,133 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

 

>Does it must input MIPI clock continuously?
yes, non continuous clock mode is not supported by i.MX6 MIPI-CSI.

 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
1,134 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

 

>Does it must input MIPI clock continuously?
yes, non continuous clock mode is not supported by i.MX6 MIPI-CSI.

 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,134 Views
takayuki_ishii
Contributor IV

Hello Igor,

Thank you for your quick response.

I will answer it to my customer.

Best regards,

Ishii.

0 Kudos