clev6630b with nfc reader library in low power mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

clev6630b with nfc reader library in low power mode?

707 Views
michaell
Contributor I

Hello,

I have dev kit CLEV6630B and I want to run it in low powered mode.

Am I correct that default example NfcrdlibEx1_BasicDiscoveryLoop is already runs low powered (passive poll mode)?
I'm not sure what consumption I should expect?
I need microAmpers, is it doable?

Regards

0 Kudos
1 Reply

559 Views
Kan_Li
NXP TechSupport
NXP TechSupport

We have an app note on that topic, for polling without LPCD, the average current is around 5mA, and around 17uA with LPCD enabled. Please kindly refer to https://www.nxp.com/docs/en/application-note/AN11783.pdf  for more details.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos