LPUART support in MQX for K65

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPUART support in MQX for K65

631 Views
yossisarusi
Contributor I

Can not see the support of the LPUART in the MQX 4_2. 

Do I miss something.

Thanks

0 Kudos
1 Reply

483 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Yosef Sarusi

     LPUART is supported in MQX 5.1. But it is under commercial license. Please check the following link for more details.

https://www.nxp.com/docs/en/release-note/MQXRN.pdf 

MQX™ v5 Software Solutions|NXP 

If you want to use MQX 4.2 with lpuart, I would suggest you make it by yourself. It is possible to merger a bare metal driver into MQX, however you need to take care about the hardware initialization, some hardware is already initialized in BSP code therefore cannot copy-paste your bare mental code.

You also can refer to lpuart driver in KSDK package, and port it to MQX 4.2.

Regards

Daniel



-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos