Hello, my problem is that I use this project UART/interrupt and compiled and debugged truly but there is no output and in debug, it doesn't go to the program and main, why?
please help me
in IAR and NXP LPC1788
Hi mino simpson,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi jeremyzhou,
Thank you for your answer, but my problem is not resolved.
I used the project that you sent. when I remove startup file, debugger goes to main and then to UARTSend but nothing was sent that I think this is because of removing startup.
when I add it, debugger doesn't go to main.
Also I changed device name in general option to lpc1788.
Hi mino simpson,
Thanks for your reply.
I'd like to indicate the testing process I did.
1. Assure the configured Device is LPC1788
2. Change the value of UART_TEST_NUM to select the J25 as the Serial port.
//#define UART_TEST_NUM 1
#define UART_TEST_NUM 0
3. Debug.
Obviously, the demo works well, I don't encounter the phenomenon you mentioned.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
problem solved, thank you very much:)