How to connect external 32.768K crystal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to connect external 32.768K crystal

ソリューションへジャンプ
1,351件の閲覧回数
alex_li
Contributor II

We want use external 32.768k crystal as RTC clock source.How to connect it to s32k142 ?

PTA7 as RTC_CLKIN, one of PTC4,PTC5,PTD13 as RTC_CLKOUT, is it right?

We also need provide 32768Hz signal to other device,can we connect it to RTC_CLKOUT directly?

Thanks!!!

タグ(1)
0 件の賞賛
1 解決策
1,043件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

It is not possible to connect a 32.768kHz crystal to the RTC module. However, you can use an external oscillator (32.768kHz) connected to RTC_CLKIN pin. This clock can be then output at RTC_CLKOUT pin for other external peripherals.

Regards,

Daniel  

元の投稿で解決策を見る

2 返答(返信)
1,044件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

It is not possible to connect a 32.768kHz crystal to the RTC module. However, you can use an external oscillator (32.768kHz) connected to RTC_CLKIN pin. This clock can be then output at RTC_CLKOUT pin for other external peripherals.

Regards,

Daniel  

1,043件の閲覧回数
alex_li
Contributor II

Daniel :

      Thanks for your explanaion!

Regards,

min li

0 件の賞賛