Hello all....
My development board FRDM - K64F board was not functional properly, I thought the old board was faulty so I requested for a new board.
I connect my new board and I can see it in the Device Manager (COM 4), when I try to connect to Putty Emulator I get an error message, unable to open serial port.
I have updated Windows driver with mbedWinSerial_16466, done a bootloader update with 0244_k20dx_bootloader_update_0x8000.bin
I tried running 'hello world' and in the workspace no probes found. The only way to get my LED on is to have it in bootloader mode.
Now I don't want to return the board, how can I sort this problem.
Do I need to install any drivers or change any settings ?
Please help... refer to attachments.
Yours sincerely
Kofi
Hello Kofi,
1. What about your PC system ?
2. If win7, please do as below steps:
1)Press the Reset button (and keep it pressed) while power the board with the OpenSDA USB connector(J26):.
2) The board will show up as BOOTLOADER drive on your system:
3) Copy" JLink_OpenSDA_V2.bin "(I attached it for you) to the BOOTLOADER driver:
4) The copy operation takes about 2-3 seconds, after finished , unpower the board.
5) Power the board again normally .
6) Change to a new workspace , open a new demo project to have a try.
If still have problem, please contact me .
Hope it helps
Alice