Hello Friends,
I am Using JN-AN-1162 Application Note.
in that i am using DEVICEREMOTE.C file to write my code.(shows in Picture)
in that "PRIVATE void vAppMainLoop(bool_t bWarmStart) "
above function act like main loop. this is restart loop after every 20sec i calculated.
this creating problem for me. in description its says that it is in NON CONTROL MODE which repeatable.
AND in Control mode it single time slice will work.
please suggest me.
i am really stuck in this situation.
Thank You for your Time
Hello mario_castaneda,
is that mean i need to change my All Application program...it will not support my previous application..
or
it just change website name?
Hi Dheeraj,
I recommend to change a new protocol, JenNet-IP is no longer supported. This protocol is using an old stack so, Zigbee and Thread are a better option for a new design.
Best Regards,
Mario
Hello Mario,
Need your help,
i am stuck at data transfer between Coordinator and sleeping device.
i don't know how to start... and no one is replying from this forum.
Please need your help.
Thank you for your time!
Hi Dheeraj,
if it is sleepy then please to refer to JN-AN-1219.
Let me know if you have issues running this AN.
Regards,
Mario
Hello Mario,
Please see attached file so you will understand what is happening.
Thank You
hello Mario,
Sorry
i didn't tell you which Application i am using .
I am using JN-An-1229 ZPS application Note.
in which i have achieve Data transfer between Sleeping Device---> Coordinator.
and its work very well.
from Yesterday i was trying to communicate vice versa.
and it happened .
but
1)only one Char is passing rest are shown blank on Sleeping Device Terminal Window.
2) and data sending and receiving only ONE Time.
only these issue i m facing right now.
Thank You for your reply