iMX6UL无法识别USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6UL无法识别USB

1,677 Views
hongyan
Contributor I

iMX6G2D  OTG1无法识别USB

MODE1=0   OK

MODE0=1   OK

USB-OTG1=3.3V   OK

USB_OTG1_VBUS=5V  OK

UART1_RX上拉10K  OK

32.768KHZ ,24MHZ  OK

VDD_SNVS_IN=3V  OK

VDD_HIGH_IN=3.3V OK

VDD_SOC_IN=1.35V OK

USB_OTG1_DP=2.8V  NG 正常是0V

Labels (1)
Tags (1)
0 Kudos
2 Replies

846 Views
hongyan
Contributor I

USB 识别错误 Unknown  Device

0 Kudos

846 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Hong Yan,

   For the issue you encoutered, see below, please!

(1) Usage of  USB OTG on i.MX6UL

   Although there are 2 USB OTG ports on i.MX6UL, only one of them can be configured to be OTG(Dual Role device), the other must be configured to HOST. They can't work at OTG mode simultaneously.

(2) Resistance for USB differential line.

   According to your description, it is also possible to cause the issue because of unmatched resistance of USB differential line. So suggest you check PCB layout. Generally, hardware engineer should use "MCZ1210AH900T" on USB differential line to match resistance .


Have a great day,
TIC  weidong sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos