Can I set the max USB link rate to USB 1.0 (1.5Mbps) in the USB 2.0 host controller port?
If I can set, can you tell me how to modify source code on Yocto 2.1?
Thank you.
Best Regards,
Alex
Hi charles
speed selection is described in sect.7.1.5.1 Low-/Full-speed Device Speed Identification
USB 1/2 specification found on usb.org, it is handled in hardware and seems there is no way to
change it in software.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------