Please advise How to cancel ECO signal on Receiving pin of the TDA5051A when is transmiting ? so far it looks like is normal to receive the ECO but can you please advise if there is a way to avoid it or cancel?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Please advise How to cancel ECO signal on Receiving pin of the TDA5051A when is transmiting ? so far it looks like is normal to receive the ECO but can you please advise if there is a way to avoid it or cancel?

715 Views
manuelmaximilia
Contributor I

Please advise How to cancel ECO signal on Receiving pin of the TDA5051A when is transmiting ? so far it looks like is normal to receive the ECO but can you please advise if there is a way to avoid it or cancel? BR  Max Ariza

0 Kudos
2 Replies

626 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Manuel,

The Data_In pin of the receiver board is pulled HIGH to 5V to disable TX in receiver.

This can be confirmed in UM10422 for the TDA5051A demo boards, see transmission test setup in Table 3 of this document: https://www.nxp.com/docs/en/user-guide/UM10422.pdf

pastedImage_2.png

Have a great day,

Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

626 Views
manuelmaximilia
Contributor I

Hello Jose

Thanks for you support !

Best regards

Max Ariza

Field Application Engineer

Manager

PLEASE NOTE, MY EMAIL ADDRESS HAS CHANGED

Arrow Components México, S.A. de C.V.

Mobile2 +52 1 55 1885 9330

Mobile2 +52 1 656 130 9261

www.arrow.com<http://www.arrow.com/>;

De: reyes

Enviado el: miércoles, 20 de septiembre de 2017 11:24 a.m.

Para: MANUEL Ariza <maximiliano.ariza@arrow.com>; MANUEL Ariza <maximiliano.ariza@arrow.com>

Asunto: Re: - Re: Please advise How to cancel ECO signal on Receiving pin of the TDA5051A when is transmiting ? so far it looks like is normal to receive the ECO but can you please advise if there is a way to avoid it or canc...

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Please advise How to cancel ECO signal on Receiving pin of the TDA5051A when is transmiting ? so far it looks like is normal to receive the ECO but can you please advise if there is a way to avoid it or cancel?

reply from Jose Alberto Reyes Morales<https://community.nxp.com/people/reyes?et=watches.email.thread> in Other NXP Solutions - View the full discussion<https://community.nxp.com/message/945016?commentID=945016&et=watches.email.thread#comment-945016>

0 Kudos