How to Boot the MCIMX6Q-SDB Boards?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Boot the MCIMX6Q-SDB Boards?

581件の閲覧回数
yaochen
Contributor I

Today, I generated mirror image of board using bitbake, based on the L3.10.53_1.1.0-ga version of tutorial Freescale_Yocto_Project_User's_Guide.pdf. And I also have produced the SD card. Next are some pictures of SD card:

QQ图片20170823222512.jpg

QQ图片20170823222518.jpg

But when I have inserted my card in board and adjusted SW6 to 0100 0010, the board didn't have any reaction. But the touch screen showed the time to finished the image. And when I connected my computer screen to HDMI interface, the screen also didn't have any reaction. Next are some pictures of board:

QQ图片20170823222427.jpg

QQ图片20170823222450.jpg

QQ图片20170823222500.jpgQQ图片20170823222507.jpg

So how should I do? And whether if I have made any mistakes?

PS:

I connected my board to host computer with minicom software. Next are some pictures:

2.png

1.png

I don't know why the instruction stopped there("raise: Signal # 8 caught")

These pictures show my Configuration of minicom:

3.png

4.png

ラベル(1)
タグ(3)
0 件の賞賛
1 返信

375件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you download image to the card by mfgtool? the default display is lvds, if you need to use other display, you need to change in the uboot command, for your "raise: Signal # 8 caught" error, suggest to use the command as below:

"

=> sf probe

=> sf erase 0xc0000 0x2000

"

if still failed, try to format your sd card, then download the image to SD card then try again, your sw6 setting and minicom setting are both correct.

0 件の賞賛