MCP5775 SDPLL can't lock when using external clock source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCP5775 SDPLL can't lock when using external clock source

465 Views
hqliu
Contributor I

Hello,

I'm using a 3.3v LVCMOS external clock source to drive MPC5775 now. The PLL0 can lock normally, but SDPLL can't lock. The code will always pending on while(AFE.PLLSTS.B.LOCK == 0); 

The PLLSTS register show 0 on bit0, bit1, bit2 and bit15.

The code can lock correctly on the same board with a crystal. The only difference on code is  AFE.OSCCTRL.B.EN_EXT setting.

Would you please let me know that if I missed something to set?

0 Kudos
0 Replies