Range issues with TVDD set to 3.3V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Range issues with TVDD set to 3.3V

830 Views
daviddevereaux
Contributor I

Hello, we are having range problems with the CLEV6630B v2.0  at TVDD = 3.3V during LPCD.  Are there registers or something that we can change to improve the sensing range.  we have changed the ON and OFF time and set the I and Q thresholds to 0.  At TVDD = 3.3V we need to wipe our card on the antenna to wake it up.  At TVDD = 5V it seem to work a lot better.  

We need our product to run at 3.3V and are wondering if there are other configuration changes to be made.  

David

0 Kudos
1 Reply

705 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello David,

    If TVDD=3.3v, there is no better way to improve detection range of card, see datasheet :

--------------------------

To connect the CLRC663 to a Microcontroller supplied by 3.3 V, PVDD and VDD shall be at
a level of 3.3 V, TVDD can be in a range from 3.3 V to 5.0 V. A higher supply voltage at
TVDD will result in a higher field strength.

--------------------------

    So if it is possible to change TVDD to 5V, do it, please!

Have a nice day!

Best Regards,

Weidong Sun

0 Kudos