Dear team,
I would like to ask about USB connection of i.MX6DQ.
My customer wants to connect external USB HUB chip (Microchip’s USB4604) to USB OTG Controller of i.MX6DQ via UTMI PHY1.
(1)
Is it OK?
If any consideration is needed, please let me know.
(2)
The customer wants to control UTMI PHY.
Is it possible to control it from API level of OS (as a general story)?
Best Regards,
Miyamoto
Hi Miyamoto,
Regarding the i.MX side, they have UTMI compliant interfaces (with internal PHYs), but also HSIC interfaces that require external PHY. You could take a look at application note AN4589 “Configuring USB on i.MX 6 Series Processors”, available at the following link:
http://www.nxp.com/docs/en/application-note/AN4589.pdf
About the USB4604 part, please refer to the following Community thread:
https://community.nxp.com/thread/386829
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello CarlosCasillas
Thanks for your support.
The customer wants to connect USB4606 into USB OTG controller of i.MX6D/Q.
Is it possible?
I think it depends on its PHY interface.
USB4606 seems to have a USB interface(Flex PHY) instead of HSIC for up/down stream, according its datasheet.
Best Regards,
Miyamoto
Hi Miyamoto,
The i.MX6 Quad/Dual have one OTG and one Host controllers with internal UTMI PHYs, and two Host controllers with HSIC interfaces. It is shown on Figure 1 of application note AN4589:
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------