imx6ul dual ethernet mdio on fec1issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul dual ethernet mdio on fec1issue

2,160 Views
Blackrose
Contributor I

Dear all:

I use imx6ul chip on our custom board.I reference the imx6ulevk board sch and code, the mdio on fec2.In this case, the fec2 is eth0, fec1 is eth1.Now, i config the mdio on fec1 pinctrl.But the eth0 and eth1 always show device not found.And i know the mdio is share with fec1 and fec2.

I search an patch for imx28, it said use FEC_QUIRK_SINGLE_MDIO can use mdio on fec1 or fec2 anytime.I try it, but failed.Here is the patch url:

[PATCH v2] net: fec: fix MDIO bus assignement for dual fec SoC's 

 

Is it the fec driver can not support mdio on fec1 at dual ethernet case?

Labels (2)
0 Kudos
3 Replies

1,252 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Blackrose,

Rather than the driver, it is not possible to use the 2 FECs with one single MII / RMII / RGMII interface because the pins are connected internally to each FEC.


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,253 Views
Blackrose
Contributor I

Thanks.I doesn't found those note on datasheet of chip.

0 Kudos

1,253 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Blackrose,

It is not quit explicit but you can infer it if you look at in the Reference Manual at Table 22-1. ENET1 External Signals and Table 22-2. ENET2 External Signals.

Here you can see that most of the signals are available in only one pin, and this pin has no Mux options.


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos