MPC5744P eTimer measurement demos check

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P eTimer measurement demos check

366 Views
nathan_
Contributor IV

Hello,

I am learning to use the eTimer module of MPC5744P to measure the duty cycle of PWM.

I want to use the port A[1] and port A[2] for measurement and I do not want to use it for 32bit counting capability, just 16bit is enough. So I found the demo named "eTimer_measurement_630", which is in the attachment, and made some changes and try to make a new demo which is fit for my requirement. the new demo is also in the attachment, named "eTimer_measurement_for_BLDC_0704".

 

Can someone help me to check if there are any errors in my new demo? Is it correct?

 

Best regards

Nathan

Original Attachment has been moved to: eTimer_measurement_630.rar

Original Attachment has been moved to: eTimer_measurement_for_BLDC_0704.rar

0 Kudos
0 Replies