SGMII 10/100 on P2020

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGMII 10/100 on P2020

581 Views
toddreed
Contributor I

When using SGMII 10/100 on the P2020, is the output based on a slower clock instead of the 625Mhz clock?

Thanks,

Todd

Labels (1)
0 Kudos
3 Replies

445 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The P2020 SGMII signal  has fixed rate in according to the SGMII specification. To support 10 Mbps and 100 Mbps data rates, SGMII stretches the frame by replicating each frame byte 10 times for 100 Mbps and 100 times for 10 Mbps

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

445 Views
toddreed
Contributor I

Thank you Serguei.  So, with the replicated data,  would it look like 62.5 mhz or 6.25 mhz data on the line?

Todd

0 Kudos

445 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

It will not look like 62.5 mhz or 6.25 mhz data on the line. The SGMII signal  has fixed bit rate.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos