At power on ebdf and others are not updating . clk out is 18.75MHz instead of 37.5MHz. Modck is 11 at power on reset. If we see in debug mode PLPRCR ( EBDF) is 00 only instead of 01. Data bus(0:15) transitions are as per configuration set values with respect to Hard reset, but not latching into the processor. PLL is locking to 18.75MHz/75mhz. Please clarify. Once in a while it is locking to 37.5mhz and immediately to 18.75mhz.
Please connect TRST pin to ground directly or via strong (1K or less) resistor and check again.
Have a great day,
Alexander
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
trst is pulled down to 1kohm. also tried by connecting gnd to trst. Problem remains same. If i see hard reset config values in view registes by connecting tab. It is showing wrong values.SIUMCR it is showing all zeroes. If i activate the debug by connect. hardreset should not generate .But it is giving hard reset also. If i load the configuration file it is not giving hardreset. i am able to run the code in debug mode.why hardreset is coming in debug connect case,though it is accessing internal register.