Hello,
My board uses a P1013 with 64 bits of DDR3 memory with ECC, and I would like to suppress memory chips to have only 32 bits access + ECC. This is for cost and consumption purpose.
Thus I have modified the config in this way :
Register @0x2110 : DDR_SDRAM_CFG.[DBW] = '01' (32 bits mode)
Register @0x2110 : DDR_SDRAM_CFG.[8_BE] = '1' (8 burst length)
Nevertheless this new conf doesn't work : bit [D_INIT] of DDR_SDRAM_CFG_2 register is stuck to 1 after the enable of the controller.
Does anyone know if I have to change other registers in order to have a functionnal 32 bits conf from a 64 bits one ?
Thanks a lot,
Jérôme
Original Attachment has been moved to: init_DDR_32bits.cmm.zip
Solved! Go to Solution.
It is also required to set SDRAM Mode Register 0 - MR0[BL]=0b00 (Fixed BL8).
Example:
If for 64-bit bus the DDR_SDRAM_MODE value is 0x00021421, then for 32-bit it has to be 0x00021420.
It is also required to set SDRAM Mode Register 0 - MR0[BL]=0b00 (Fixed BL8).
Example:
If for 64-bit bus the DDR_SDRAM_MODE value is 0x00021421, then for 32-bit it has to be 0x00021420.
Hello, It works fine with the fixed BL8 value ! Thanks a lot !!
Jérôme