for the BOOT_CFG3[2] setting of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

for the BOOT_CFG3[2] setting of i.MX6

Jump to solution
517 Views
yuuki
Senior Contributor II

Dear all,

I have a question about Boot constitution pin of i.MX6.

The BOOT_CFG3[2] selects a frequency for ARM and DDR until Boot loader in the Boot device is executed.
  0 - ARM - 792 MHz, DDR - 396 MHz, AXI - 264 MHz
  1 - ARM - 396 MHz, DDR - 352 MHz, AXI - 176 MHz

I understand that after Boot Loader was executed, they(ARM/DDR/AXI) work in a setting value in Boot Loader.
(all PLL is set again by Boot Loader.)

Is my understanding right?


Best Regards,
Yuuki

Labels (2)
Tags (1)
0 Kudos
1 Solution
402 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes this understanding is right

Best regards
igor
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
403 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes this understanding is right

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos