IMX6Q Solution Standby Power Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q Solution Standby Power Problem

400 Views
ygzhou
Contributor I

Hi all:

       We are now using the IMX6Q platform program, on the issue of standby power to ask a few questions:
1. Test the entire machine sleep the minimum power consumption is 58mA, I would like to know why the minimum power consumption will be so high, which will be the reason?
2. Many other programs are the lowest power consumption of 5-10 MA, and IMX6Q standby power consumption is high, why is there such a big difference?
3.IMX6Q program standby minimum power can do how much?
Thank you

0 Kudos
1 Reply

323 Views
igorpadykov
NXP Employee
NXP Employee

Hi

for power consumption in low power modes please check AN4509

i.MX 6Dual/6Quad Power Consumption Measurement

https://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf 

Pay aatention measurement procedure described in

sect.2.7 Measuring Points on the Freescale SABRE SD Board

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos