Hi pgo,
please check the 4.12.1.150 because it can´t program the MC9S08JM60CLD. The programmer can detect chip but can´t program or erase it, returns TCL error when try "mass erase now" or "program flash" I loaded the flash image USBDM_JMxxCLD_V4.sx from FlashImages folder. The option "verify flash" works fine. I am using windows7 64bits. I try some commands on TCL interpreter and it works.